2025-06-10 4:52 PM - last edited on 2025-06-11 1:32 AM by Andrew Neil
I'm looking for CAD resources of NUCLEO-H755ZI-Q board Revision D-01. Currently en the web-page there are for revision C-01.
Thanks
Solved! Go to Solution.
2025-07-01 2:25 AM
Hello,
Update, design files for rev D01 should be there:
2025-06-10 7:22 PM
It could be that there are no changes to the PCB. You could compare the two BOMs and see what the difference is/are. That would take some time though. It would be nice to have a list of Engineering Change Notices (ECNs) on the schematic or elsewhere.
2025-06-11 1:00 AM
Hello,
>> It could be that there are no changes to the PCB
If the revision has moved from C to D, that means PCB has been changed. It could be minor (like silkscreen) or not.
I have entered an internal ticket #211945, to see if it can be added.
2025-06-11 1:35 AM
I see both Revision D-01 and C-01:
2025-06-11 1:42 AM
>> I see both Revision D-01 and C-01:
Maybe I'm wrong, but I understood the request was for "MB1363 Board design project files" and "MB1363 Manufacturing files" which are only for Rev. C, because, as you mentionned, schematics for rev C and D are there.
2025-06-11 1:51 AM
Maybe: @Lupillo_1788 just said, "CAD resources" - didn't say what "resources", specifically.
But the BoM, Manufacturing, and Design files are all dated after the D01 schematics ...
2025-06-11 6:45 AM
2025-07-01 2:25 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.