2020-08-17 7:03 AM
On Windows 10, I just updated (again) to the 1.4.2 version, hoping to solve this issue, yet nothing changed.
Already tried a clean install (again) and re-installed the latest STM32CubeProgrammer: nothing changed.
Will ST handle this sooner or later please? Or at least give some help in diagnosing the problem? Thanks
Solved! Go to Solution.
2020-08-27 2:42 AM
Hi, yes indeed I tried MS32, didn't think of trying also the MinGW as I thought they were the same no matter the compiler...
2020-08-28 7:41 AM
Hey,
Same issue here on mac, did you have a patched .dylib version for MacOS?
2020-08-28 8:15 AM
2020-09-01 3:49 AM
Awesome thanks heaps.
2020-09-01 5:46 AM
Did it work on Mac Os with this newer libusb version ?
2020-09-01 8:17 AM
I patched the libusb inside the folder and it didn't work initially. So I clean installed 1.4.0 from the site and updated again to 1.4.2 and it works perfectly now.
2020-09-03 1:21 PM
Oops! Did you do the new istall and then patched the libusb file inside the folder? And secondly, in what folder?
Thanks for reply.
Have a good day.
2020-09-24 9:23 AM
Hi LaurentL,
can you describe where to put the mentioned content of the file macos_libusb, please. (I assume after after extracting) I am not that familiar with computer insides ... I searched on my Mac for older files like that, but could not find a path, which makes sense to me. I only found the path Macintosh_HD/usr/local/lib/ ... connected to an older file of the name libusb-1.0.0.dylib ...
Thanks for reply.
Have a good day
Andreas
2020-09-24 9:34 AM
Hi,
I don't know the MacOs file system.
But from TahaS's answer, it seems he didn't have to patch the lib but more to do a clean install 1.4.0 and then update to 1.4.2.
Try that before patching the libusb.
Rgds,
Laurent
2020-09-30 8:59 PM
:downcast_face_with_sweat: Me too:
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.