Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
i have STM32103RBT6, i want to use all three UARTs for a project. i want to use UART2 thorugh PA2 and PA3. The connection are : SB61, SB62 and SB63 are open. SB13 & SB14 are open as well. Continuity is there between SB62 & SB62 to TX on ST link (from...
Two STM32H743 series MCUs are on a single board and they communicate using SPI. When SPI clock frequency is more than 1.5 Mhz, SPI communication is not working properly. The distorted clock signal waveforms at high frequencies are attached below.A 51...
Hello everyone,I have designed a custom board using the STM32F407VGT6, and I have connected a 3V coin cell battery (CR2032) to the V_BAT pin as shown in the schematic below:V_BAT Circuit Details:A 3V battery is directly connected to the V_BAT pin.A 0...
Hi sir, I am Sridhar from Sirveen stm32f746g-discovery board Datasheet is not given Operating temperature details. So please provide clarification or provide link for download including temperature readings datasheet please.
Hello.. anyone can advise where to find user manual and schematic for Discovery kit for STM32H750? I would like to know if H750 Disco is using Ethernet MII or RMII? I was looking at F750 Disco is using RMII. TQ!
Hi I am trying to send data from the ISM330DHCX sensor to BLE (BlueNRG-M2SA) on the STM32F401 Nucleo board. I have installed the XCUBES_MEMS1 software and successfully tested the LED example via BLE. Now, I want to transmit the ISM330DHCX sensor data...
Hi community,Where can I buy the STM32F407-DISC1 and Nucleo-F446RE boards in Morocco? Can anyone guide me on this?
Hello. For a couple months now, I have been trying to get the microphone on the STM32F407-g Discovery board to work. It started out as a minor part of a self-guided course, but now it's turned into a personal quest. The farthest I've gotten so far is...
When I have the HC-06 powered from the board (either 3.3V or 5V) & try to upload to the board I get, Target no device foundError in initializing ST-LINK device.Reason: No device found on target. Yet when I unhook the module from the board everything ...
I'm trying to receive data through USART1 using STM32F407. I decided to not use HAL api's to achieve that, so I'm receiving character by character and storing them in an array. Every character I send is received correctly but apart from the actual da...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.