STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! stm32u575 & Ethernet port

Hi,I've a board, now a nucleo-u575zi-q but i'm waiting for a custum boad based on same MCU. I need this serie for the low power functionalities. In next phase of project , in this board i need an ethernet port where run web and tcp server. I found so...

mauroalba by Associate II
  • 3704 Views
  • 8 replies
  • 2 kudos

Resolved! STM32h753x - JTAG interface

We are planning to use STM32H753X in one of our design. For JTAG interface I can see two options 5 pin and 4 pin JTAG. Is STM32H753 supports 4 pin JTAG? If yes, how to manage NJTRST pin? Shall i connected NJTRST pin to NJRST?  what is the use of 5 pi...

DJ_IND by Associate III
  • 1476 Views
  • 1 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.