2025-04-01 2:31 PM - last edited on 2025-04-02 12:57 AM by Andrew Neil
Hi,
Could you list NUCLEO-H753ZI board's ADC1/2 ADC3 channel Index with GPI/O Pin assignment table with the connector name / pin index on the board, using channel number as the index
It is very difficult to configure CUBEMAX-ADC without this Table. Especially, some ADC pin(s) may not be accessible on this board. I appreciate if you can provide this table:
ADC1/2 Example
Channel Index GPIO NUCLEO Board Connector Index Connector Pin Index Sharing Info
IN3 PA6 CN8-D12 (Pin 7) with ADC3_IN12
ADC3 Example
Channel Index GPIO NUCLEO Board Connector Index Connector Pin Index Sharing Info
IN2 PA2_C CN8-A2 Pin 9 with ADC1/2_IN14
Thanks,
Rong
2025-04-16 8:07 AM
Hi @RongShengWang ,
Where exactly do you suggest to have such information?
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.