Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Hi, I have recently purchased a STLINK-V3PWR with the intent of using it to measure power consumption on my board. Previously I used STLINK-V3SET's JTAG port (MB1440 CN2) to connect to my target board.The STLINK-V3PWR only comes with STDC14 connectio...
Hi, Are there any EV (Evaluation) boards available that support GPS functionality? Thank You
Hello everyone,I’m currently working with the STEVAL-PROTEUS1 evaluation kit. According to the User Manual, the board features a 34-pin, 0.4 mm pitch high-current connector for board-to-FPC or board-to-board expansion. It is stated that: “The pinout ...
My board has the C031C6 nucleo, my attempts were:Change the USB for a data cable;Try to connect with the under reset and software reset on the Programmer;Update the firmware and driver on the Programmer, IDE and ST-LinkUpgrade;All of this with and wi...
Trying to get SPI1 to work on the NUCLEO-H7S3L8.Starting a new project from the Board Selector works with no problem, however starting from the MCU Selector, the HAL_SPI_Transmit gets stuck at in stm32h7rsxx_hal_spi.c in the while loop at line 4008.E...
I'm trying to create an ADC project using nucleo-h723zg. I want to measure AC voltage and current (simultaneously). I created electronics with isolation amplifiers, which have, as an output, a differential signal with a common DC voltage. The common ...
Hi,I'm designing a PCB using H755, and the corresponding Nucleo's reference design is a helpful resource that I've been looking at closely.I'd like to support supply config modes 2 & 3 on my board but would prefer to do this using jumpers rather than...
Hello, I am an engineer developing a board using STM32G071. Currently, I am using all pins of the MCU, SPI, I2C, and GPIO, but one of the products is overheating and overcurrent is occurring. The existing consumption is 30mA, but the problematic pr...
Hi ,I am using NUCLEO-H723ZG board for my project work. It was working fine and from few days I am facing an issue, when I try to debug or try to run the code an error pops up telling : Error in initializing STLink device. Target no device found.
Please keep the title short - less than 1 line. Edited.Hello,currently i looking for some suggestions with regards developments or evaluation or nucleo boards for the given controllers:STM32F205RET6STM32F303C8T6 if anyone is currently working or havi...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.