STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Power leds are blinking

 Hi I don’t know the reason, but my board’s ld2 and ld8 leds are blinking, and the program says  No STLink detection, even if I connect it to the usb port, what can be its reason? How can I fix it?

IMG_7491.jpeg
MÖZDA.1 by Associate II
  • 935 Views
  • 6 replies
  • 0 kudos

STM32H755BIT3 Supply connection

你好 我正在与 STM32H755BIT3 一起做项目。我设计的电路板的现状是,用DC-DC 3.3V电源上电后,芯片很快发热严重,不出现短路就无法下载程序。我推测这是由于外围电路的设计。 有人可以帮忙找出问题所在吗? 提前感谢大家的任何提示。 Translation: Hello I am working on a project with the STM32H755BIT3.The current situation of the board I designed is that after...

LLionel by Associate
  • 1188 Views
  • 1 replies
  • 0 kudos

Resolved! ST_LINK can not connect to target

Hello, I've been trying everything for days to fix this error. They said to set the BOOT0 pin to GND. I followed these steps. I tried many solutions from YouTube videos and the STM32 website, as well as solutions from forums, but none of them worked....

bekos by Associate II
  • 992 Views
  • 7 replies
  • 3 kudos

Resolved! How to use multiplexing port.

Hi all.I'm using STM32H747I-DISCO bord.According to user manual, Pin No.1 in Pmod™ is connected to PA11/PA0.And Pin No.1 in STMod+ is also connected to PA11/PA0.Then can I use PA11 as USART1_CTS via Pmod™ Pin No.1, and PA0 as GPIO via STMod+  Pin No....

Paco by Associate III
  • 416 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.