2015-03-25 10:25 PM
Hi,
I'm using IAR EWARM 7.3. I'm using ST-Link, newest firmware. The target is connected via JTAG. It flashes and seems to run OK - the IWDG is ticking fine without crashing, with RTOS running. I can print using ITM_Sendchar(). The Debugger option is set for ''Connect during reset'' After launching the application, there are 2 odd things happening. First, when I try to stop the application (Red X) I get the pop-up dialogue that says ''Target is running, Failed to stop the target'' The other is the SWO trace output. Each time I run the debugger, it does not ''save'' the trace output settings I have to keep checking the boxes for ITM0 output. Any suggestions? I could not find anything in the forums... Thanks. #stm32f4 #st-linkWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.