Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
st link is unable to connect with stm32f103r8 in my circuit board, while programming using keil the nrst pin becomes low when debug is applied and unable to program, but using IAR & ST link utility unable to connect to the microcontroller, board is p...
I'm currently using an STM32L4 on a custom board, trying to implement is a composite USB class that allows CDC and MSC at the same time. I am working with the STM generated classes for CSC and MSC, and have written an intermediate composite interface...
After a redesign of the PCB, STM32F401RB is not recognized by the PC when connected via USB. There is no change on the USB Connections. There are 22R resistors connected in series with the USB data lines. Is this issue related to the value of the res...
Hi Experts, I'm using STM32F407 MCU, in a bot where I have seen ESD due to (friction/movement) in the bot, and this ESD reset my MCU several time unexpectedly.So I would like to know an ESD protected reset circuit for the board any other suggestions ...
ST-LINK utility connects normally and the target reacts as expected to its Run / Halt / System Reset buttons.Clicking Run or Debug from Workbench causes the target to become unresponsive. The target recovers by subsequently reopening/connecting ST-LI...
Hello,I am designing a custom hardware for STM32L051K8U6 microcontroller but I am not getting the reference design for the mention controller. Please share the link for the design if I missed it.Thank you
Hello Team,We are evaluating 32L4R9IDISCOVERY reference design for our wearable device development.While exploring BOM we found that the AMOL OLED[MPN : IEG1120TB103GF-001] [datasheet attached] which is used in the evaluation kit is not more availabl...
Hello Team, We are evaluating 32L4R9IDISCOVERY for one of wearable device.While checking obsolescence we got to know that the Pseudo SRAM used with it i.e., IS66WVC2M16ECLL-7010BLI is facing unconfirmed lead time.As a cross reference to IS66WVC2M16E...
According to AN4661 "Getting started with STM32F7 Series MCU hardware development ":"When the voltage regulator is enabled, VCAP1 and VCAP2 pins must be connected to 2*2.2 μF low ESR < 2 Ω ceramic capacitor. In the STM32F7x2Rx devices, only the VCAP1...
Hi folks,I am trying to set the RDP option bytes to have my code in flash read-protected. Instead of using ST-Link Utility, I want to set the read-out protection in the code itself (specifically, inside a self-designed bootloader). For this purpose, ...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.