STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Touch sensing design

Hello all,i have a problem with my first design of a touch button and a slider on a 4layer pcb (top-layer2-layer1-bottom) using a STM32L162 with its peripheralTouch sensing. As you can see from the image i have design the button and the slider with a...

ypkdani by Associate
  • 1099 Views
  • 0 replies
  • 0 kudos

ST-LINK V3 firmware upgrade failed

I am using Ubuntu 18.04 VirtualBox on MacOS with STM32G484QE-EVAL baord. While switching to STM32CubeIDE 1.1.0, the debug tool will ask to upgrade the STLINK V3 firmware. Clicking the upgrade button and "STLinkUpgrade 3.3.0" will start. Click "Open i...

0690X00000Aqr6VQAR.png 0690X00000Aqr6aQAB.png
JasonZ by Associate II
  • 2068 Views
  • 3 replies
  • 0 kudos

Cannot connect to STM32L4R9I - Disco

Hi, every one, I am new in STM32. Recently, i got 2 STM32L4R9I - Disco. the first one work perfectly fine. as i plug the STLink to connect the first one to the Laptop. it works and the connection also appear on Device manager. i can load and debug th...

Hi, while debugging STM32F072 I am facing some issues as below, At time of debug I am getting Debug warning as verify error from address onwards 0x08003800 application code size is reach just around 20KB,and controller enters in hard fault.

At time of debugging my application card based on stm32f072 controller I am getting Debug warning as verify error from address onwards 0x08003800 & and controller enters in hard fault. Current application code size is reach just around 20KB In case I...

Power Nucleo from User USB

Hello,as the title tells, I would like to power up a Nucleo 144 board (STM32l496) from its User USB connector. I've read the documentation and it tells that it is not possible, but would it remain impossible even with an external regulator connected ...

Resolved! STlink debugging hardcoded to start at Reset_Handler address ignoring vector table values.

STM32F030R8Blank project, no CMSIS, no Cube libraries.Code copied from my old TrueStudio project.I use old startup_stm32f030x8.s with some modifications.If I change startup vector table start entry to my function (named not Reset_Handler but Boot_Sta...

AOmel.242 by Associate II
  • 1873 Views
  • 2 replies
  • 0 kudos

ST Utility External Loader Example

Hi everyone,I have to write a custom external loader and reviewed the examples. The read text of these examples say that after the folder placed inside cube files, it will run seamlessly. However, I can't do this, it needs lots of files to build. Ple...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.