2019-10-20 5:27 AM
STM32F030R8
Blank project, no CMSIS, no Cube libraries.
Code copied from my old TrueStudio project.
I use old startup_stm32f030x8.s with some modifications.
If I change startup vector table start entry to my function (named not Reset_Handler but Boot_Start), then
compiler works OK,
elf contains correct vector table
downloads and runs OK
BUT
debugging by ST-Link (with unchecked "Resume" in Startup Debug Configuration settings):
debugger shows my function (OK)
disassembler window shows my function (OK)
BUT
PC register is set to Reset_Handler address (or junk if no such symbol)
and attempt to step or run will go to bad address.
Well,
I can rename my startup function into Reset_Handler and old Reset_Handler (I will jump there in the end) in some Old_Reset_Handler. Then I can debug my bootloader and my application.
Nevertheless it's an IDE Bug.
(TrueStudio performed OK in that case).
Solved! Go to Solution.
2019-10-20 7:54 AM
You are right,
readelf shows entry point set to Reset_Handler, not to my routine, despite to correct vector table.
I,ve changed setting in .ld file, and now it is ok.
So, it is not Bug.
I'm sorry.
Just different behavior re. TrueStudio.
Of course, it would be nice for debugger to inform us about inconsistency of elf header and vector table.
2019-10-20 7:30 AM
Check entry point exported in .ELF header
2019-10-20 7:54 AM
You are right,
readelf shows entry point set to Reset_Handler, not to my routine, despite to correct vector table.
I,ve changed setting in .ld file, and now it is ok.
So, it is not Bug.
I'm sorry.
Just different behavior re. TrueStudio.
Of course, it would be nice for debugger to inform us about inconsistency of elf header and vector table.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.