STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! V1.1.0, segger j-link support gone?

Hi I installed STM32CubeIDE V1.1.0 and now I can't select J-Link as a debug probe, only ST-link (GDB & OpenOCD).I get the J-link if the project was created in an older STM32CubeIDE version, but not in the new 1.1.0.Any hints on how to enable J-link?

ST-LINK cannot connect my device

Hello There,I dont know if this is the right place to get help. I am a newby and working with STM32H747I DISCO.Currently ST-LINK cannot connect my device. I did the following troubleshoot based on online solution.==> Update stlink utility==> Pull boo...

STM32H745I-DISCO Board- I'm using IAR Workbench v 8.40.1 and the ST-LINK V3 shared mode does not work. I assume you need this mode to do dual-core debugging.

Has anyone been successful in enabling and using dual-core debugging of this H745I-DISCO board using the on-board ST-LINK v3 interface? I am able to use the interface to dowwnload and debug each core separately; however, I can't get the ST-LINK sh...

stm32f09 command line programming issue

issue-when programming using the Command line utility it indicates success but the unit does not boot.  when programming from the GUI the unit powers up correctly.  I used the same command line on an st32f07 without issue.  Here is the command line.​...

STM32CubeIDE - ST-Link GDB Slow

HiI am starting to develop a new project using the STM32F469I-Discovery Board using the TouchGfx library.I am using the CubeIDE (v1.1.0) and trying to use the ST-Link GDB Server for debugging. The ST-Link is taking a very long time to download a new...

Resolved! I cant able to load the code Because Over Current (RED) LED is glowing on my STM32H743 Micro Controller . What is the cause and What is the solution for it so that i can load the code again ?

Hello,Iam using STM32H743 Nucleo board.Suddenly The Red LED (Over current LED) is glowing in my Micro controller. I have cheked all the connections properly there is no short circuit in it. Because of this i cant able to load the Program in it It is ...

MGane by Associate II
  • 5710 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.