STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Connection failed when trying to connect STM32L053R6T6 using STM32 ST-LINK Utility Version 4.50 as a latest version.

When we connect STM32L053R6T6 using STM32 ST-LINK Utility Version 4.20, it works normally.But when trying to connect it using STM32 ST-LINK Utility Version 4.50 as a latest version, it fails.Please refer to the attached files.Please let us know how t...

STM32L071 Programming error @: 0x08080C08

HelloWhen I use ST link utility for programming STM32L071 error occur when it starts to program EEPROM. Each time first 8 bytes are programmed correctly and after that an error occur. After that it's not possible to change EEPROM bytes manually from...

lgoti by Associate
  • 1018 Views
  • 0 replies
  • 0 kudos

ST-Link Utility with STLink/V3

I am trying to program write ST32L051 boards with stlink utility and stlink / v3 in auto mode, but the v3 probe does not recognize the board's SWD port. Of course, firmware updates and drivers are up to date.Is it related to the firmware version of s...

hkwak.1 by Associate II
  • 2852 Views
  • 6 replies
  • 0 kudos

Change SPI MOSI-MISO Pins

Hello,I am using STM32L100 in one of my projects. I designed a PCB for this and it appears that I made a mistake on the layout. SPI's MOSI and MISO pins are not correctly routed on the PCB layout they are just opposite of how they should be connected...

herca.1 by Associate II
  • 5502 Views
  • 4 replies
  • 0 kudos

STM32 Nucleo32 Dev Board I/O Current Limit

Are the STM32 Nucleo-32 dev boards IO pins rated for 50mA? I couldn't find any information about the max ratings of the IO pins for the dev boards. I need them to be rated to up to 5V, and be able to output 50mA of current. If this is not possible, w...

KChan.3 by Associate
  • 8044 Views
  • 4 replies
  • 0 kudos

Failed to execute MI command

HIThis is my first time using ST environment and ST-LINKI have encountered an Failed to execute MI command. Below is the log file.Could someone please point me in a direction where to start to looking for a solution.ThanksSTMicroelectronics ST-LINK G...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.