Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
I wrote my program and I try to debug it. In first execution I had a specific timing but if I stop code, I reset it from Debug tag all timing are double fast... so any comunication became impossible.If i didn't use debugger without ST LINK connected ...
I am designing a schematic for my project which uses the STM32F779BI microcontroller. I am using the LQF208 package of the microcontroller. The symbol of the microcontroller is available at different websites but during the schematic design of the mi...
Hi!!Do you know any adapter from lqfp144 to DIP format so you don't have to solder in SMD?Thanks.
I have developed External Flash Loader for STM32F756 & Cypress Chip.I could compile my code in IAR. Also updated device info in file.Then I copied that file in External Loader folder.But I could see only a some blank spaces in some fields please guid...
st-link server does not install on MAC OS Catalina.messageThis package is incompatible with this version of macOS.
Summary of the problem:Basically, the firmware seems to "skip" some lines of code when I run directly after programming, while if I perform a hard reset through the board button I get the firmware behaving as expected.My setup:My test board is the ST...
Hello, I would like to ask you one question.In the datasheet of NUCLEO-L432KC, MCO output from ST-Link MCU should be used for input clock of L432KC MCU to use/enable HSE option.I wonder if I can use HSE without using MCO output from ST-LINK MCU.I wa...
Hi,In the STM32F103RDT6 , The datsheet showing VDDA pin needs 10nf AND 1Uf. But in AN2586 reference document, it shows 100nf and 1Uf. which one is correct?Warm regards,Monisha OM
I am using Stm32 f446re nucleo-64 with stm32cubeide but haven't connected the board yet, to solve the above problem I tried installing St-link stsw-link007 and St-link stsw-link009 the st-link/v2 driver but even that didn't help . please suggest a pr...
We were using Micron NOR flash with STM32F756 as given in EVAL board.In ST Link we were using option "M29W128GL_STM32F756G-EVAL" for external loader.Now we have replaced Micron NOR Flash with Cypress NOR Flash.But above mentioned option is not workin...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.