2019-12-02 8:23 AM
HI
This is my first time using ST environment and ST-LINK
I have encountered an Failed to execute MI command. Below is the log file.
Could someone please point me in a direction where to start to looking for a solution.
Thanks
STMicroelectronics ST-LINK GDB server. Version 5.3.2
Copyright (c) 2019, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
LogFile Name : C:\Users\Marius\STM32CubeIDE\workspace_1.0.1\RobotisCR1\Debug\st-link_gdbserver_log.txt
Logging Level : 31
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Enabled
SWD Debug : Enabled
Target connection mode: Attach
Hardware watchpoint supported by the target
COM frequency = 24000 kHz
ST-LINK Firmware version : V3J4M2B3S1
Device ID: 0x449
PC: 0x80014c8
ST-LINK device status: HALT_MODE
ST-LINK detects target voltage = 3.28 V
ST-LINK device status: HALT_MODE
ST-LINK device initialization OK
Waiting for debugger connection...
Waiting for connection on port 61234...
Accepted connection on port 61234...
Debugger connected
Enter STM32_AppReset() function
NVIC_DFSR_REG = 0x0000000B
NVIC_CFGFSR_REG = 0x00000000
XPSR = 0x01000000
------ Switching to STM32CubeProgrammer -----
-------------------------------------------------------------------
STM32CubeProgrammer v2.2.0
-------------------------------------------------------------------
Log output file: C:\Users\Marius\AppData\Local\Temp\STM32CubeProgrammer_a12024.log
ST-LINK SN : 001B002C3137510839383538
ST-LINK FW : V3J4M2B3S1
Voltage : 3.27V
SWD freq : 24000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x449
Device name : STM32F74x/STM32F75x
Flash size : 1 MBytes
Device type : MCU
Device CPU : Cortex-M7
Memory Programming ...
Opening and parsing file: ST-LINK_GDB_server_a12024.srec
File : ST-LINK_GDB_server_a12024.srec
Size : 5740 Bytes
Address : 0x08000000
Erasing memory corresponding to segment 0:
Erasing internal memory sector 0
Download in Progress:
�������������������������������������������������� 0%
�������������������������������������������������� 100%
File download complete
Time elapsed during download operation: 00:00:00.520
Verifying ...
Read progress:
�������������������������������������������������� 50%
����������������� 35%��������� 53%��������� 71%
Error: Data mismatch found at address 0x08000B44 (byte = 0xD7 instead of 0x04)
Error: Download verification failed
Encountered Error when opening C:\ST\STM32CubeIDE_1.0.1\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_1.1.0.201910081157\tools\bin\STM32_Programmer_CLI.exe
------ Switching context -----
Error in STM32CubeProgrammer
Debugger connection lost.
Shutting down...
2020-01-10 3:55 AM
Hi,
I have the same problem. Have you or someone found a solution?
It seems a problem only of CubeIDE, bacause ST-Link Utility flash the microcontroller without failing the verify.
Best regards
Lorenzo
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.