STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Design of ST hardware

I want to design hardware with STM32G071RBT6 micro-controller, i have basic design circuit but i want to build strong power supply with reverse polarity protection and industrial noise free hardware. please provide me solution for Hardware design.

This is a specific question Programming a new IC STM32030 using an ST-Link and STM32CubeProgrammer. I have spent considerable time trying to understand why I cannot connect to my stm32. I have attempted to connect and program through STM32CubeIDE also.

The St_link registers itself and the serial is updated etc. however when I attempt to connect to the newly soldered chip, I get the message that "No STM32 target found".Am I attempting to program this chip incorrectly by using the SWDIO, GND, SWCLK a...

0690X00000DXP7KQAX.jpg 0690X00000DXP7FQAX.jpg 0690X00000DXP7AQAX.jpg
BMcCa.1 by Associate
  • 1647 Views
  • 3 replies
  • 0 kudos

STM32L152RE Schematic Verification

I am trying to create custom PCB for my academic project. This is the first time i am using an STM32 processor. I will be grateful if someone can verify the schematic for STM32L152RE which i created.I will be using SWD to flash code to the STM32. The...

0690X00000DXRzYQAX.png

Resolved! prebuilt Altium design files for the STM32G4 series?

Hi guys - Any idea how long it will take for prebuilt Altium design files for the remarkable STM32G4 series to show up? [I am specifically designing for the STM32G431RBI6, which is a tidy 5mm x 5mm BGA with 8x8=64 balls @ 0.5mm pitch.]. I don't know ...

TB by Associate III
  • 2145 Views
  • 2 replies
  • 0 kudos

Resolved! Stm32f042f6 tssop package , when i am powering ,microcontroller is not starting ,even if i use hard reset . its only starting when i connect ST link( SW Debug)

YStm32f042f6 tssop package , when i am powering, microcontroller is not starting ,even if i use hard reset . its only starting when i connect ST link( SW Debug)  mode.I am using external clock 8 mhz.I have attached Circuit diagram !! i tried with cou...

SKira.1 by Associate II
  • 2344 Views
  • 2 replies
  • 0 kudos

Resolved! Updating STM32H743 Nucleo from ST-Link to J-Link

Has anyone succeeded at it? What did you have to do? I've found a lot of success stories about updating the ST-Link on 32F4 boards but none on the H7. When I run stlinkreflash.exe I always getPreparing for FW update (can take up to 10 seconds)...ERRO...

n2wx by Senior
  • 3997 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.