2020-02-22 12:17 PM
YStm32f042f6 tssop package , when i am powering, microcontroller is not starting ,even if i use hard reset . its only starting when i connect ST link( SW Debug) mode.I am using external clock 8 mhz.
I have attached Circuit diagram !! i tried with couple of MC but still same problem..
Solved! Go to Solution.
2020-02-23 7:46 AM
PB8 is also the BOOT0 pin. You either want to add a pull-down here to ensure flash boot mode or override that feature by programming the USER option bytes in flash.
2020-02-23 7:46 AM
PB8 is also the BOOT0 pin. You either want to add a pull-down here to ensure flash boot mode or override that feature by programming the USER option bytes in flash.
2020-02-25 7:24 AM
Thank you !! Now its working!!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.