STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I had a problem with STMF334R8, I loaded the same program on several boards with some STLINK V-2, via CubeIDE and then I was unable to get them to connect again to the computer to load another program with any kind of st link. What could cause that?

I had a problem with STMF334R8, I loaded the same program on several boards with some STLINK V-2, via CubeIDE and then when I tried to conect the MCU's again to the computer i had an error: failed to initialize GDB server, and in the console it appea...

XZuri.1 by Associate
  • 1019 Views
  • 2 replies
  • 0 kudos

Resolved! STM32L4P5G-DK

DISCO board for the new 'L4Pxx is out:https://www.st.com/en/evaluation-tools/stm32l4p5g-dk.html?icmp=tt14426_gl_****_mar2020#Remarks:yet another naming scheme, with -DK suffix - bad idea, DISCO was a good keyword to search these at the distributorsno...

STM32F412CGU6 ESD Issues

Hi, We have a product based on a STM32F412CGU6 MCU that is currently going through certification. Are there any known ESD issues or knwn reasons why the MCU would tend to latch up? We are seeing this behaviour and can't get to the bottom of it.Thanks...

LArcu.1 by Associate
  • 628 Views
  • 0 replies
  • 0 kudos

Resolved! Proper powering of STM32` MCU on a custom PCB

Hello guysI am developing my own PCB where I want to use a STM32F767 MCU. I went ahead and figure out how to load binary and all but there is one thing that confuses meso from the schematics (datasheet) my MCU has more than one VDD and VSS (ground) I...

hashtala by Associate II
  • 1870 Views
  • 4 replies
  • 0 kudos

Resolved! I not to able programming the NUCLEO-H743ZI2

I have an NUCLEO-H743ZI thats works fine. So now i have buy a new NUCLEO-H743ZI2. With the samge Firmware i not able to programming the flash. I have upgrade the ST-Link V3 with the latest FW. But nothing helps. When i try to programming the Flash i ...

CDrey.1 by Associate II
  • 2996 Views
  • 5 replies
  • 0 kudos

Mounting an STWLC68 (WLCSP72 package)

Hi, I am new to working with BGA components this small. Are there any particular issues (solder paste composition, paste type, avoiding caffeine, etc.) that I should consider? I want to be able to reflow some prototype boards myself before having any...

MReev.1 by Associate
  • 706 Views
  • 0 replies
  • 0 kudos

STM32F105 USB without VBus sensing

I want to make USB which is operating in Device mode to enable pullup and pulldown resistors and reset without built-in VBus sensing pin. I've tried HAL_PCD_DevConnect(&hpcd_USB_OTG_FS) but it didn't work.How can I command USB to start working ?

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.