2020-10-24 11:11 AM
I have STM32H750 100pin chip and STLINK-V3MINI. Pin 9 of mini 14 pin connector has no obvious place on the chip. There is already a JTCK/SWCLK signal between 6/14 and PA14/STM32H.
I am using AN4938 table 6 and UM2502 also table 6 to connect debug pins.
Solved! Go to Solution.
2020-10-25 8:14 AM
On the typical ARM 10-pin, that's the KEY pin (missing), perhaps there is a JTAG variant of the cable/connector where this is the same as JTCK, or it provides a second clock for another chain/device.
I'd focus on SWCLK, SWDIO, SWO and NRST signals.
2020-10-25 8:14 AM
On the typical ARM 10-pin, that's the KEY pin (missing), perhaps there is a JTAG variant of the cable/connector where this is the same as JTCK, or it provides a second clock for another chain/device.
I'd focus on SWCLK, SWDIO, SWO and NRST signals.
2020-10-25 10:20 AM
Yes, I have SWCLK, SWDIO, SWO and NRST signals handled. T_JCLK is just last "unhandled exception" in that connector.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.