STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! No ST-LINK detected! - Nucleo H723ZG

Hi,So far I was using Nucleo WB55 and everything was ok with ST-LINK. Now I created new project and switched to Nucleo H723ZG. When I try to run or debug I receive message:No ST-LINK detected! Please connect ST-LINK and restart the debug session.The ...

0693W00000AMjfcQAD.png 0693W00000AMjfhQAD.png
DPiór.1 by Associate III
  • 7591 Views
  • 6 replies
  • 0 kudos

Clock source selection for stm32f767

I am planning to use stm32f767 mcu. I am confused to use clock for the same. I am referring discovery board schematic but in that NZ2520SB-25.00M is used for MCU and Ethernet controller. In my case i won't be using ethernet. I will be using TFT inter...

SS.Sagar by Associate III
  • 2131 Views
  • 1 replies
  • 0 kudos

Hello, I have a wired mouse connected to STM32F407 discovery board and i followed your steps in the tutorial but it did not work. Could you please let me know what is the hardware connection required to achieve this setup?

Should pin PA9 needs to be connected to something on the board and is there any way to call the eventcallback function.My main issue is that the wired mouse is not asensed by Vbus.Its voltage is 0V. Could you please help me on this.Any help would be ...

SShub.1 by Associate II
  • 2095 Views
  • 3 replies
  • 0 kudos

STM32L4R5 debug port hardware connection

Hi, I'm trying to design the STM32L4R5 IC on my PCB board and use the STLink V2 as the debugger. Should I use the SWJ or SWD debug port options? What are the pros and cons for both?Since the STLink V2 is a 20 pin JTAG connector, how do I connect the ...

CYeow.1 by Associate II
  • 1699 Views
  • 2 replies
  • 0 kudos

Resolved! STM32F407 First Programming Failed

Hello Community!I have a project where I was using a STM32F407 MCU from a minimal ready-to-run system with USB, programming connection and pin headers to access every MCU pin. While using this hardware, the project can be loaded and executed on the M...

ÀTorr.1 by Associate
  • 1495 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.