STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Hello, I am new to STM32 and keil µvison5.I have a STM32F407VGT6 I wrote a code and it's build successfully . But when I try to load ,it says "NO ST-LINK detected "Cannot enter debug mode" and "Error:flash Download Failed-Target DLL has been canceled"

I reinstalled everything from keil to the st-link utility. I reinstalled the driver en.stsw-link009 . But still the same problem. Also it's not detected by the st-link utility.So, any solutions ?

NSOLT.1 by Associate II
  • 2659 Views
  • 6 replies
  • 1 kudos

STM32L552 SMPS hardware design

I have a question about connecting of the SMPS V15SMPS pins. From the datasheet we see, that the V15SMPS_1 and V15SMPS_2 pins are connected internaly. But, on the "Figure 6. SMPS step down converter power supply scheme" they are alco connected extern...

Schematic for STM32F469I-DISCO B03

Last week I bought a few STM32F469I-DISCO boards from DigiKey. Today I wanted to look at the schematic and found that there are two revisions available, B07 from 2015 and C01 from 2020.  But I have B03!  I'm wondering how old my board actually is, an...

Resolved! STLink Utility v4.6.0 does not run

It complains about not finding mfc140.dll.I do have mfc140.dll in C:\Windows\System32.What next?JW[EDIT] The CLI does not run either, throws the same error:  After copying mfc140.dll into the directory where the stlink-utility executable is located (...

0693W00000ALzUYQA1.png 0693W00000ALzTGQA1.png

Resolved! [NUCLEO-F722ZE] EXTI15_10_IRQ

Hi,I wanted to generate interrupt on pins PC14 and PC15 on NUCLEO-F722ZE board but it doesn't work. In the board documentation I found that jumpers configuration should be as per screenshot. Since elements there are pretty small and I don't want to d...

0693W00000AM91HQAT.png
SHutc.1 by Associate
  • 1329 Views
  • 1 replies
  • 0 kudos

Resolved! Schematic for Nucleo-L412RB-P please.

I'm trying to find a schematic diagram for the Nucleo board with the L412 processor, but can't track it down. I've looked in the User Manual for this product (UM2206 rev 5) where I would expect it to find it but it isn't in there. I'm not sure if thi...

PSmit.3 by Associate
  • 1542 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.