STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

No USB enumeration anymore

Hi all,I build a prototype board based on STM32G431KBT6 which need Virtual COM port and DFU firmware upload. In previous version of the prototype everything worked fine.Windows detected the board, I was able to send/receive commands over VCP and also...

0693W00000AOPZ9QAP.jpg 0693W00000AOPZiQAP.jpg
WSpar.1 by Associate III
  • 1827 Views
  • 3 replies
  • 0 kudos

I/O pin internal short to VCC

Can desoldering and soldering to replace a capacitor which is part of an RC filter of an I/O pin cause that pin to develop an internal short to VCC? This problem has now happened on 14 PCBAs. Any insight would be gratly appreciated. Regardsik

IKhan.2 by Associate II
  • 1910 Views
  • 2 replies
  • 0 kudos

Resolved! Computer isn't detected the BluePill (STM32F103C8T6) board on windows 10. Can anyone help me to solve it?

Hi,I am quite new in this MCU world and I bougth a BluePill board (STM32F103C8T6) to start doing the basics and learn.At first I tried to use the IAR Embedded IDE to program the board but when I tried to debug the following error appears.Then I tried...

0693W00000AOV5ZQAX.png 0693W00000AOV6cQAH.png
JLode.1 by Associate II
  • 5030 Views
  • 4 replies
  • 0 kudos

STM32H725IGK6 Boot Issues

I'm using STM32H725IGK6. I come from Microchip PIC world.When pulling up 'BOOT0' with 10kΩ to VCC(3.3V) , I'm able to run my code on my custom designed board using STM32CUBEIDE.When I press RST or power cycle board, nothing runs. This is expected rig...

KRega.1 by Associate II
  • 3096 Views
  • 3 replies
  • 0 kudos

Need STLD40D substitution

Hi,Is there, by any chance, a substitution for the white LED power supply for large display blacklight used in the STM32H45I-DISCO LCD schematic ?The product have 0 stock everywhere and will be available in 20 weeks. I can't wait that long to test my...

ANaud.1 by Associate II
  • 1409 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.