Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Hello,I'm planing to design a custom board using STM32F769 and I want to use the STM32F769I-DISCO as a reference but I didn't manage to find the PCB files in the CAD Resources section of the said product. There are only schematic packs, BOM and gerbe...
Hi, I'm trying to connect a joypad through COM3 and I don't get what kind of pinout & configurations should be made in order to connect this joypad for coding. I'm new in developing a program using stm32, so if you could explain it in detail about th...
Facing some problems related to emulation circuit in STM32MP157C-DK2. STM32F103CBT6 micro-controller used in this application requires firmware i.e. STLinkv2/1. Please provide the hex file for firmware-STLinkv2/1 and necessary details to program the ...
The same board was created based on the stm32f469i_Discovery board. The stm32f469i_Discovery board operates st-link/v2 using the stm32f103.Please let me know if you know which program to put in the stm32f103 and how to put it in order to operate the ...
위�? 언급�?�었�?� 보드�?� 회로�?�를 찾�?� 수 없습니다.구글�?과 �?��?�터시트를 찾아봤지만 찾�?� 수 없었습니다.보드 사용하기 위해서 회로�?�가 필요하니 회로�?�를 참조 할 수 있는 주소나 파�?��?� 있으면질문�? �?�져있는 주소로 보내주시면 �?사하겠습니다.***Moderation Edit: please do not post your email address on this website***
HelloI have created a prototype board using STM32L476RE.Then I did "Target" > "Connect" in ST-LINK utility, but I got the error as shown in the picture.I do not know the cause and solution. I did a lot of research on this site and checked the followi...
I'm using a Nucleo-F746ZG with timer 2 as a quadrature encoder input. I'm feeding it quadrature signals from 2 GPIOs at 250Hz (each phase is 1mS).The CDR value is 0, so FDTS should be CLK_INT (36MHz for APB1). With both inputs' filter set to 8, the...
My team has built up a complex test setup with about 72 ECUs of which all have an ST Link V2 connected to update all the controllers automatically.With the help of an USB extension board they are all actively connected to the PC. The issue is now, th...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.