Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
I have recently bought a stlink v3 mini and I have connected with STM32F103C8 (blue phill) board with SWIO, SWCLK, and Gnd. I tried to upload a blink program many times. But it says failed to start GDB sever and no device found on the target and I ...
HI!I made a custom board with STM32G474RC. Unfortunately the ST-Link V2 cannot connect to it. I have two pices of V2. (Bought from local store but probably clones.). This is the message I get: "No STM32 target found!" Tried it with CubeProgrammer, U...
Dear ST expert,STM32G474 serials are very good option on digital power control, and I see the WLCSP81 package is pretty small(only 4mmx4mm). I plan to use WLCSP81 package on 1/4 bick power module which is 12 layers and the topology is Hard Switch Fu...
Hello, I would like to integrate STLINK-V3MODS into my own board, but I can't find the internal schematic of STLINK-V3MINI or MODS anywhere.Is it possible to obtain MB1467 schematic?Thanks
Hello, i want to create a custom board for stm32 h7 series and run Free RTOS on it for a specific application. Which is the most advanced debug i can use to ensure i get all the correct debug tools on the market for this project both software and har...
Hi, I'm using a STM32L100RC discovery board and I'm trying to send/receive words through the Virtual Com Port (VCP). Nevertheless, even after installing the STM32 Virtual COM Port Driver (STSW-STM32102), the board is not connected as a VCP but as a U...
I just got an MCUDEV board for the STM32H743 chip. I have been using an eval board and have my code configured in the CubeIDE. When I connect the MCUDEV board to my computer via a Micro USB to USB cable, LED D1 turns on and LED D2 starts flashing. Bu...
Hi,i want to know if i did the wiring correct? The 4 x 100nF will be connected close to PIN 19, 32, 48 and 64.PIN 1 got a 1uF.On PIN 13 (VDDA) i added a bead as well.NRST will not be used in the final application, is the 100nF anyway needed?BOOT0 is ...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.