2021-05-21 6:46 AM
2021-05-21 7:35 AM
It it actually materially different or just a design refresh of an old board, with currently available parts, perhaps a newer ST-LINK implementation? And arguably obsolete. ST has been migrating away from EVAL boards as being too expensive and low volume, and moving to high function DISCO boards on current generation parts.
What information are you actually looking for?
2021-05-21 8:13 AM
Ok thanks for your reply. I was looking for some examples e.g. code of the demo application for that eval board. Unfortunately I could‘t find any examples in the stmCube IDE either. (e.g. as there are a lot of examples to be found for the STM32L552E-EV, which is also in ACTIVE state like the stm32439i-eval2 board)
2021-05-21 8:34 AM
The F4 is a decade old, the L5 is significantly more recent
Pull the CubeF4 package
STM32Cube_FW_F4_V1.25.0\Projects\STM324x9I_EVAL\Demonstrations
STM32Cube_FW_F4_V1.25.0\Projects\STM324x9I_EVAL\Examples
STM32Cube_FW_F4_V1.25.0\Drivers\BSP\STM324x9I_EVAL
@Ons KOOLI Please check status/plans for https://www.st.com/en/evaluation-tools/stm32439i-eval.html page currently broken, no discussion of EVAL/EVAL2 differences
2021-05-21 8:47 AM
EVAL2 is the one with the 5.7" 640x480 panel (as I recall there was a model with a smaller screen, 4.3" 480x272)
2021-05-24 1:45 AM
Hi @CHam.1 , @Community member ,
Thank you for reporting this. I will check for it internally and provide you with feedbacks. In the meantime, I suggest you to review in other packages (board design project file, BOM and manufacturing files) which included all the different board revisions.
Best Regards,
Ons.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.