Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
I am miniaturizing the STM32F767ZI for a project I am working on and would like to have it function identically to the standard STM32F767ZI. Part of this includes having the ST-Link aspect of the board so we can program it via USB. I have not been ab...
So just yesterday I programmed/reprogrammed my custom board that has a STM32F746NGH6 MCU just fine from STM32CubeIDE. Always have programmed without any issues on 5 custom boards I made. Today (02/09/2021) on trying to download the program with a sli...
We buy original STlink v2 and we hawe problem with connect to STM32L451CCU6. On china programator MCU connect all time. On STlink connect time to time and if we are connented we can't program MCU. Bellow screen, first china programator, second STlink...
Since STM32 STLINK Utility Command Line Interface has return codes, why STM32Cube Programmer don't have?
Hi! I have this problem with my STM32F401RE and STM32G431RB when i connect the target and try to flash my code with CubeIde, I tried to solve this using ST Link Utility, CubeProgrammer, upgrating drivers but nothings works, my G431 firmware isn't re...
Hi there, we are currently designing a sandwich board for the STM32H747i-DISCO board and we want to connect via CN8 and CN5. So far I have only found technical drawings in dm00504240.pfg (see attachment). But the exact position of the two connectors ...
I get an error pop up saying "Error in final launch sequence: and Failed to start GDB server?How do I troubleshoot this error?
Hi,I couldn't find the pcb.doc of the 32F769IDISCOVERY board. Would you please send the PCB files ?Thanks
In reading the manuals and datasheets, it seems like it should be possible to simultaneously use all 3 channels (DAC1 Channel 1, DAC1 Channel 2, and DAC2 Channel 1) of the onboard DACs at once, emitting separate values on each. However, no matter wha...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.