2021-11-08 11:45 PM
I would like to use the stlink/v3 on the Nucleo144 stm32h7a3 board to program/debug my board is this possible? what do I need to connect?
2021-11-09 12:54 AM
Hello,
I advise you to download the nucleo board schematic to know witch connections are used. Board reference is MB1363 you can download schematics here: MB1363 - Resources - Search STMicrocontrollers
Connector CN5 is an easy way to connect a board to STLinkV3.
BR
Chloé
2021-11-09 1:22 AM
I used the cn2 in this way from the left 3v3, swclk, gnd, swdio towards the pins of my card pin 3 (swclk), pin 1 (gnd), pin 4 (swdio) and pin 6 (3v3). when I connect it to debug to my program it tells me no device found on target
2021-11-09 2:09 AM
You also need UART to work. signals T_VCP_TX and T_VCP-RX are available on CN5 connector.
2021-11-09 6:01 AM
I don't see an easy way on that board to disconnect SWDIO/SWCLK from the onboard processor. You would need to do that before using it to program an external board. The VCP connections are definitely optional.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.