STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How should I do a power cycle?

Which Pin should I set and reset to make a power cycle happen in STM3G4 or any popular STM32F3xxx.. ??I have 2 mcu's and with one of it I want to do a power cycle..I mean to remove the power and connect it again. What should I do here?

Vmere.1 by Senior
  • 5537 Views
  • 10 replies
  • 0 kudos

RMII GPIO state after HAL_ETH_Init()

Hi,we have a PHY with several bootstraps. Some of them are shared with the RMII from a STM32H753 (see image below, controller is on the left).A FreeRTOS+TCP network stack is used, which, when rebooted, first does some low level inits with HAL_ETH_Ini...

0693W00000Hred2QAB.png
DWeb_2 by Associate III
  • 2492 Views
  • 3 replies
  • 0 kudos

Resolved! JTAG and UART connectivity

Hello,We working on custom board. We using this controller STM32745IIkx. In JTAG we connect the USART1 port, but there is pin mapping issue, so I am unable to use USART1.So instead of UASART1 can I use USART2.I am sharing its schematic THE VCP_TX and...

0693W00000JMKZzQAP.png
MDeva.1 by Associate II
  • 3166 Views
  • 4 replies
  • 0 kudos

Hi, I bought a Nucleo STM32F401RE board. Yeasterday the board was working fine in dimming led in A0 pin which was configured in PWM mode. Now I can't reprogram the board. See details for error message. PS. I'm a total beginner with microcontrollers

Starting server with the following options:    Persistent Mode      : Disabled    Logging Level       : 1    Listen Port Number     : 61234    Status Refresh Delay    : 15s    Verbose Mode        : Disabled    SWD Debug         : Enabled    InitWhile...

VNisk.1 by Associate II
  • 5450 Views
  • 10 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.