cancel
Showing results for 
Search instead for 
Did you mean: 

Hi, I bought a Nucleo STM32F401RE board. Yeasterday the board was working fine in dimming led in A0 pin which was configured in PWM mode. Now I can't reprogram the board. See details for error message. PS. I'm a total beginner with microcontrollers

VNisk.1
Associate II

Starting server with the following options:

    Persistent Mode      : Disabled

    Logging Level       : 1

    Listen Port Number     : 61234

    Status Refresh Delay    : 15s

    Verbose Mode        : Disabled

    SWD Debug         : Enabled

    InitWhile         : Enabled

Target Held under Reset

Error in initializing ST-LINK device.

Reason: Target held under reset.

This discussion is locked. Please start a new topic to ask your question.
10 REPLIES 10
Imen.D
ST Employee

Hello @VNisk.1​ and welcome to the Community :)

Is BOOT0 pulled LOW?

Check the power VDDA​, and don't pull NRST low.

If a post answers your question, please close this topic by choosing "Select as Best" on that post.

This will help other users find that answer faster.

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
VNisk.1
Associate II

At the moment there is nothing connected to the Nucleo board.

I' will try to connect the BOOT0 to GND.

Should I let the NRST be unplugged or connect it to 3,3V?

What do you mean with "check power VDDA"?

TDK
Super User

"Target held under reset" suggests NRST is being held low. You should not be connecting this pin to anything, and certainly not driving it to 3.3V.

Can STM32CubeProgrammer connect?

If you feel a post has answered your question, please click "Accept as Solution".

The STM32CubeProgrammer connected when I set the ST-Link mode: Hot plug. Still the Full chip erase fails.

Other modes have the same problem as earlier descriped.

I tried connecting BOOT0 to GND.

(CUBE programmer with SWD, normal, hardware reset)

Error: No STM32 target found!

So the problem still exists?

Piranha
Chief II

Use "Connect Under Reset" mode.

VNisk.1
Associate II

I tried that. Still getting the same response: "Error: No STM32 target found!"

Should the be a 3,3 voltage in NRST pin. as far as I can tell the pin is low all the time. (Connected it led without resistor and still nothing).

Do you think the board maybe faulty?

A multimeter would be a better test. The pull-up is small and may not visibly drive an led.
If you feel a post has answered your question, please click "Accept as Solution".
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.