Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Hello, Im trying to power this board and sensor with 30mA power consumption @ 5V with 5V output of the board. What im noticing is the board is not capable of mantaining the voltage with this light consumptions. It starts at 4.7-4.8v with nealy 0mA co...
Hi allI tried to flash the code stm32f469i board i am getting this error please check below,IDE i am system workbench stm32.
I have a device that needs I2C and several GPIO from the discovery board, I found all the signals on P2 (STMod+) connector on my discovery board. The connector itself is designed to connect STMod or an other custom board to the discovery board. In my...
But What It's mean exactely ? I must buy a Debugger like ST-LINK/V2 ? Thank you for your helps. Regards
I am able to connect in SWD mode and debug target hardware but am unable to flash images to target by overriding Flash loader with my .board file in "Debugger->Download" optionKeep getting following warnings and no flash download occurs:Wed Dec 12, 2...
Trying to identify the best temperature profile to ensure an optimum solder flow and resulting solder connection.
Dear Support Team,I have problem with STM32F105RBT6 overheating,After several months of operation, the processor will break down, overheat and burn out completely.Power consumption is constantly rising, but it works flawlessly even with higher power ...
Hello, I have some project with RTC. Initially project was made with STM32F405 uC, now all porting to STM32F765 uC. Problem with RTC, on the new board with F7 uC I have error around 2 sec per day, where board f405 - I have error 1 sec in 4-5 days. B...
I did a fresh install of STM32CubewMX and STM32CubeIDE. I built a simple program that does nothing except configure an LED to turn on as part of the GPIO initialization. Try as I might, I can program it when trying to debug, but cannot debug. Excerpt...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.