2022-04-28 6:31 AM
2022-04-28 6:54 AM
It is not that things aren't being produced, it is that they are immediately sold, or pre-sold, and aren't sitting on some dusty shelf at a retail distributor.
Found a couple of listings on eBay this morning, and bought half a dozen..
Bunch more on AliExpress
2022-04-28 6:57 AM
Perhaps your local ST FAE or rep can find you some?
2022-04-28 7:05 AM
We are a very large, very bureaucratic company. We are working with registered suppliers only.
They do not have this device in stock for at least a half year and they have no idea when it will be back in stock.
My team can't work without it
2022-04-28 7:53 AM
I'm familiar with the company, want consumer level product/pricing (COTS), but months of paperwork for a handful of devices, and the process repeats in 12-18 months because the consumer level product has done a design refresh, or cost reduction cycle.
You should probably work directly with ST, or their supplier in China (probably WaveShare)
Alternatively, if it is critical, you could probably just manufacture it yourself and licence the design/firmware. Or commit staff to implementing the JTAG/SWD programming protocols to your level of satisfaction. The Flash cell programming is achieved in exactly the same way as a user program would, here with code/data is pushed into RAM and executed by the micro-controller.
The performance of the flash cell programming is primarily dictated by the voltage and temperature. For integrity a SHA-256/SECP192R1 is reasonably robust.
2022-05-05 8:46 AM
Hi @Zoycha ,
To answer your initial question: The STLINK-V3SET is still in production. All the quantities provided to ST distributors are rapidly sold, so that we are currently working with our subcontractors to increase outputs with new units available in one month.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2022-05-06 8:24 PM
You may be able to find V2's which may work for you, or failing that, use the programming section of nucleo 64 boards for a V2.
2022-05-08 9:32 PM
Hi @Amel NASRI
Thank you very much for your answer.
But in fact, I do not understand what is so special about this model that it is so requested worldwide.
Do you have any estimates as to when that might be available?
Thank you again
--Zoya
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.