STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Am working on NUCLEO STM32F401RE , so after debugging the code, am facing this issue. Please advise for this, so i can work speedy. Target no device found Error in initializing ST-LINK device. Reason: No device found on target.

STMicroelectronics ST-LINK GDB server. Version 7.0.0Copyright (c) 2022, STMicroelectronics. All rights reserved.Starting server with the following options:    Persistent Mode      : Disabled    Logging Level       : 1    Listen Port Number     : 6123...

kabid.1 by Associate
  • 1304 Views
  • 1 replies
  • 0 kudos

STM32L452RET6 Question

Hi all,I am using the STM32L452RET6 On my board and i have 2 quiestion regarding it:1) VDD12 Net - how to set my hardware when i am not using external DC/DC? floating? GND? just a cap? if so what size?2) when entering boot mode and going over the i/o...

iHamd.1 by Associate II
  • 3024 Views
  • 6 replies
  • 0 kudos

STM32 Boards and USB Host issue

Hi,I'm trying to make a simple USB host for MSC devices. I'm working with a STM32F429 NUCLEO-F429ZI board and a STM32F407 STM32F407G-DISC1 boards.The matter is that both boards have USB power switches wih oppostie logic. That is, the Nucleo boards ha...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.