2022-09-16 3:58 AM
STMicroelectronics ST-LINK GDB server. Version 7.0.0
Copyright (c) 2022, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
InitWhile : Enabled
Target no device found
Error in initializing ST-LINK device.
Reason: No device found on target.
2022-09-16 5:45 AM
Hallo @kabid.1 ,
I advise you to refer to this FAQ: How to solve debugger connection issues.
Check if all jumpers are correctly configured.
Try using latest release of STM32Cubeprogrammer, and make sure to upgrade the ST-LINK/V2-1 firmware.
Try connect to "Under reset" mode.
When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.
Imen
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.