STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! I'm trying to connect to a custom PCB made using an STM32L552ZET6Q using SWD and Cube Programmer, but I keep getting the "No STM32 target found!" error.

I've gone over the hardware with a multimeter and all the pins have the right continuity, I've checked the design against the Nucleo-144 L552ZET6Q schematic and it checks out so far, and I've also checked the connections to the ST-LINK/V3 pins I'm us...

ESpra.1 by Senior
  • 6089 Views
  • 21 replies
  • 0 kudos

HyperBus (OctoSPI) length matching

I'm doing PCB layout and I'm trying to assign pins for the HyperRAM (HyperBus) that will give me the simplest layout.The app note for the RAM IC has extremely strict length matching requirements. For example, matching between the data lines all have ...

STM32F4 Hardware for external clock

I want to develop my own PCB using STM32F4. I want to use one external clock (16 MHz). I wonder where I have to connect the clock: OSCIN32-OSCOUT32 (pins 3 and 4) or OSCIN-OSCOUT (HSE) (pins 5 and 6 in STM32F446RET).I can see in the development board...

DElec.1 by Associate II
  • 5948 Views
  • 7 replies
  • 0 kudos

Resolved! Warning: The core is locked up

For our device, we are using STM32H750 IC. in some 100 PCBs manufactured at our company, in 1 or 2 PCBs we cannot program the blank MCU and get this warning in STM32CubeProgrammer. "Warning: The core is locked up"What can be the issue? any specific p...

dv.13 by Associate II
  • 18688 Views
  • 8 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.