STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F446RET6 - can't program it through SWD

Hello,I received my STM32F446ret6-based PCB for my student project, PCB was already assembled from the JLCPCB factory and I can't program it through the SWD header with ST-link. I checked every trace on PCB with schematic and measured continuity with...

Orsen by Associate
  • 2707 Views
  • 3 replies
  • 0 kudos

Resolved! No ST-LINK detected

When I try to debug the standard led toggle example I get the No ST-LINK detected message,Board: STM32H7A3ZIT6QHost: Windows 11IDE: STM32CubeIDE 1.10.1When I open Device Manager and connect the board to USB there is not one extra device detected. I a...

Bob Louwe by Associate II
  • 2958 Views
  • 2 replies
  • 1 kudos

Why my MCU is not detected

In the picture:pin 1 top left: VDD 3.3V 4 100n to GRND 14 to GRND 15 to VDD 16 to GRNDon their left 1µ and 10n F decoupling VDDA VSSApin 32 top right : VSS 0V GRNDpin 31 10K ohm to GRND 24 SWD clk 23 SWD dio 17 to GRN...

remi2 by Associate II
  • 3833 Views
  • 6 replies
  • 0 kudos

Resolved! VCAP in hardware design

I have got a custom PCB using STM32F4. I don't have any capacitor connected to the VCAP Pin and I wonder if this is necessary or not. Which is the use of VCAP and do I need to add it to my design? What can I do to solve my problem of no having one if...

DElec.1 by Associate II
  • 14717 Views
  • 6 replies
  • 4 kudos

LVDS devices

I have two devices I am looking to integrate with STM32 MCPUs. One is a Honeywell HG1125 IMU and the other is an WFF93 Encoder.Both devices use LVDS signalling. I don't know much about that signaling at this point, but I am taking a broad stroke fi...

Hi, I would like to ask if it is possible to use NUCLEO-F042K6 to program another STM32 MCU via embedded ST-LINK? Thank you. Best regards, Ondrej

I see from the schematics in datasheet UM1956 that there is a reserved CN2 connector with SWDIO and SWCLK, NRST can be found on CN3. But I do not see any jumpers to switch whether ST-LINK is used to program on-board Nucleo MCU or an external MCU like...

OLufi.1 by Associate II
  • 1256 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.