2022-09-26 11:26 AM
I see from the schematics in datasheet UM1956 that there is a reserved CN2 connector with SWDIO and SWCLK, NRST can be found on CN3. But I do not see any jumpers to switch whether ST-LINK is used to program on-board Nucleo MCU or an external MCU like they can be found on bigger Nucleo boards.
2022-09-26 11:49 AM
No
The CN2 connects to the ST-LINK's MCU SWD pins, for programming that, not programming external devices
You'd likely need to remove the STM32F042K6 from the board, and then escape the SWD pins via PA13/PA14
2022-09-26 1:28 PM
Thank you for the clarification. I will use a different bigger Nucleo. Best regards, Ondrej
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.