STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! H753ZI USART2 debugging

Hi,I want to debug the H753ZI through USART2 and connect to the PC through USB. I've done this a lot with other NUCLEO boards. Apparently this feature is not present on the H753ZI board?Is there another UART connected to the ST-link on this board? Or...

TVan .8 by Associate III
  • 4063 Views
  • 7 replies
  • 2 kudos

the windows computer recognized the st-link v2 as universal serial bus instead virtual port

Hi.After firmware upgrade for st-link v2, windows computer recognized the st-link as universal serial bus instead of virtual com port. whenever i try to program to MCU, there is error like a "No target device found".How can I solve it?Below image is ...

ST-Link V2.PNG
kevin1971 by Associate II
  • 11693 Views
  • 21 replies
  • 1 kudos

STM32 Discovery and 5V logic

Hii hope im asking my issue in the right placeso i have developed a pcb board with 70 TLC5947 ic's in cascading sequence, however im having an issue with using my STM32 discovery board to turn on LED's. the Ic's are powered by 5V and when i use my ar...

VYada.3 by Associate II
  • 2010 Views
  • 3 replies
  • 0 kudos

Is it possible to use the generated 1.2 V of SMPS for another IC, in STM32H7 with the direct SMPS supply configuration?

I want to design a board that has an STM32H7 with internal SMPS and an SSD2828 which needs 1.2 V too.I'm wondering if it is possible to use the internal SMPS of the microcontroller to produce the 1.2 V for Vcore like the below picture and also use th...

0693W00000WLEvBQAX.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.