STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! The page with ordering still does not work

Hi Camil   All field together with Region field a fulfilled, please see picture   The page with ordering still does not work.   The error is: "Our server needs a little break while we do some upgrading to the site. Please try again shortly." I tr...

s1w_1-1707553533542.png
s1w by Associate
  • 1409 Views
  • 1 replies
  • 0 kudos

Resolved! power issue building custom mcu board

hi i have several questions about setting up STM32 chips as im trying to build a project which requires me to do so but ive encountered issues on my first step. im currently trying to set up my own MCU board using a STM32F722ZET6 144 however once i c...

Screenshot 2024-02-11 002150.png Screenshot 2024-01-29 115706.png IMG_20240211_081654.jpg
voxe by Associate II
  • 2897 Views
  • 3 replies
  • 0 kudos

Resolved! NUCLEO-L552ZE-Q using external ST-LINK

 Hi,I have a quick question that I couldn't find the answer to.I accidentally detached ST-LINK part of the NUCLEO-L552ZE-Q board https://www.st.com/en/evaluation-tools/nucleo-l552ze-q.I would like to reconnect the MCU part with ST-LINK using its SWD ...

PZdev by Associate II
  • 2149 Views
  • 2 replies
  • 0 kudos

improving progam executiion speed

To improve the execution time of a program being run on the board 'Nucleo-439ZI' from the current 20 ms period to less than 1 ms [more than 20 times reduction]. To reduce the same, I tried to switch the clock frequency source of the timer to HSE (8 M...

KumarTP by Associate III
  • 19531 Views
  • 34 replies
  • 18 kudos

Resolved! STM32F103 not working SWV

Hello here,I tried to use SWV for debug plotting in my project.I have STM32F103TBU6 and ST-Link V2.I turn on Trace Async Sw:My clock:In main.c I defined "stdio.h" and _write func:/* USER CODE BEGIN 0 */   int _write(int file, char *ptr, int len) { i...

0693W00000WLIjiQAH.png 0693W00000WLIkbQAH.png 0693W00000WLIlAQAX.png 0693W00000WLIkXQAX.png
EBurk.1 by Associate II
  • 5228 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.