Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Where is the stm32G474QET6TR pinout figure?I cannot find it in the datasheet.I need to know which pins on the board are PC3, PA11 or PB2.like this picture
Hi I have an urgent issue.I cant seem to be able to change some settings on the MCUsPCROP1_STRT 0x7FFFPCROP1_END 0x7FFFPCROP_RDP is checkedPCROP2_STRT 0x7FFFPCROP2_END 0x7FFFI cant change them. If i try i get12:32:21 : Error: Expected value for Optio...
I would like to replace the actual display available in STM32F469-DISCO with another LCD MIPI 4 Lanes (datasheet attached). Do you think that its possible to create a "wire solution" to add this new display or its require a major modification to the ...
Hello, I want to evaluate a solution using a SMT32 MCU with a TFT display (MIPI-DSI) and a camera input via DCMI.With these requirements I've restricted the MCU list to these 6 families:F469/F479F769/F779L4R9/L4S9U599/U5A9U5F9/U5G9if I am correct.The...
I just installed Cube IDE 1.15.1 on my Windows machine. When I attempted to connect to a target, it asked to update the firmware for the ST-link. The upgrade process worked, but when the pod re-booted Windows was unable to find a suitable driver and ...
Dear all, I've been looking through the datasheets, trying to find where are the pins for all of those UARTs I'm supposed to have:As seen on the picture, so far I was able to find only 1 and 7. I've also discovered 3 but haven't activated it because ...
Hello,my nucleo WL55JC1 board is not detected by cubeide when I want to run (No ST-LINK detected). The com led lights up green and with the st-info --probe command I find STM32WLEx for the dev-type. I can also update the st-link via cubeide but as so...
Hi, I am trying to connect one energy meter sensor which has RS485 output , But i am unable to read RS485 sensor readings in Nucleo F401RE, If you have any examples please help out!!
We are interfacing the USB 2.0 , on nucleo-L496ZG OTG_FS_IRQHandler routine is executing but incase of our own Hardware having LQFP64 pin package download the same code but OTG_FS_IRQHandler is not generating,may i know what is exact the issue?
I've been using my st-link for a long time and suddenly my computer stopped seeing it as st link. Please do not offer simple solutions such as updating drivers or deleting the device and reinstalling it. I installed the drivers from the official site...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.