2024-05-07 7:39 AM
I would like to replace the actual display available in STM32F469-DISCO with another LCD MIPI 4 Lanes (datasheet attached).
Do you think that its possible to create a "wire solution" to add this new display or its require a major modification to the board?
Best Regards,
2024-05-07 7:54 AM
STM32 MCU only support data via 2-lanes, this is typically enough to support 1.1 to 1.2 Mpixel displays. If your display can operate in 2-lane mode it should be workable with a suitable driver and configuration.
The STM32F769I-DISC1 provides for a Mictor connector to interface to other DSI displays. There's a converter for HDMI panels, and RPi FPC connected displays.
2024-05-07 8:06 AM
Thanks for the info @Tesla DeLorean .
STM32 MCU only support data via 2-lanes. All STM32 only support 2 lanes?
2024-05-07 10:51 AM
The STM32 MPU (Linux) models that I looked at also only supported 2-Lanes, so not going to sustain FHD / UHD type applications, so assuming about zero penetration of the tablet market space.
A subset of the STM32 MCU support DSI, might be on some of the other silicon, but only enabled/licensed on a few models and bonded to LVDS IO-Cells
At the end of the day is mostly the memory bandwidth ceiling that's the biggest hurdle.
2024-05-07 11:37 AM
The 720x1280 is 0.9 Mpixel, so I think the STM32F469 should be able to drive it via LTDC and DSIHOST
The Data Sheet has the following "Note 1 when use MIPI DSI 2-lanes, Please contact Toppan", so might need external jumper/pin setting, or configuration.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.