STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I2C Slave RX callback doesn't called

Hello everyoneI am using NUCLEO-H563ZI as master I2C, and STM32F412G-DISCO board as slave I2C, which should mimic temperature sensor TMP117.I am trying to send from master to slave a register number to read from, but the rx callback in the slave does...

MichaelR_0-1721544888128.png MichaelR_1-1721545083709.png
MichaelR by Associate III
  • 1749 Views
  • 2 replies
  • 0 kudos

Resolved! using LCD-TFT controller without HAL

Hello, i am trying to configure the on-board TFT-LCD on STM32F429-Disc0 board and i want to do it without using HAL drivers, every tutorial on youtube or other platforms i see, are using CubeMX or HAL or both. I understand we need SPI5 to configure t...

sk12 by Associate II
  • 7595 Views
  • 11 replies
  • 8 kudos

STLink V3-PWR and OpenOCD

Are there plans to add support for the STLink V3-PWR to OpenOCD?  At present, the USB device interface appears not to be supported (using the latest openocd snapshot).  STLink V3-MINIE works fine with openocd. For the V3-PWR, see the error (boldface ...

DAlbe.3 by Senior II
  • 8321 Views
  • 5 replies
  • 1 kudos

Resolved! UART on F7508-DK

I am trying to implement a data transfer using UART on the STM32F7508-DK, but cannot get it to work. I have been trying for the minimal example from the step-by-step instructions https://wiki.st.com/stm32mcu/wiki/STM32StepByStep:Step3_Introduction_to...

Jamiw by Associate II
  • 1549 Views
  • 1 replies
  • 1 kudos

Serial NOR Flash read/write operation

I need to read/write data into the external Serial NOR Flash (MX25U25645GMI00) via Quad SPI of STM32L412RB board using STM32CubeIDE.I was able to get the Device ID of the MX25U25645GMI00.I am unable to write/read data into the MX25U25645GMI0 in Auto ...

VSASI1 by Associate II
  • 3191 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.