STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! NUCLEO-H753ZI voltage output

Hello, Can I output an adjustable voltage ranging from -10V to 10V using the h753zi development board? I found something like a "PWM to 0-5V/10V DAC Module."Would I need to use such an external module or build an additional circuit externally to achi...

HMsDobby2 by Associate III
  • 1650 Views
  • 1 replies
  • 1 kudos

Programming NUCLEO-F303ZE with JTAG

Hello, I made a code to readout all the STM32 ADCs. The code works.I want to run it on my Nucleo-F303ZE with JTAG ProVision, but it dont work.What did I do wrong?I connected it like this:JTAG               NUCLEOTCK     =>        SWCLK-JTCK (PA14)TMS...

SFentro_X_1-1732893823786.png SFentro_X_2-1732893964023.png

STM32f446re Altium

Hello everyone, I’m currently working on a project involving the STM32F446RE as the main microcontroller. It’s my first time using Altium Designer, and I’ve been searching for the footprints and schematic symbols for the components I need. While I’ve...

Soniaa12 by Associate
  • 2828 Views
  • 1 replies
  • 0 kudos

Resolved! STLINK-V3MODS UART API

Hello, The documentation and flyers of the STLINK-V3MODS specify that the product includes an USB to UART bridge. My custom board with the V3MODS works for JTAG/SWD, I2C and Virtual UART. However, the documentation and sample code does not contain an...

Resolved! How to attach battery to STWINBX box?

Silly question but eyesight gets worse with age.How do I attach the LiPo battery? I do see the polarity but I just can't discern whether I shall slide the contact in from the side, or press down from above. And how do I pull it apart afterwards? Bett...

Resolved! Failed to program STM32H743ZI2 board and Debug terminal also get hang with USB isolatorfrom Linear technology

I expected to connect my PC to a nucleo STM32H743ZI2 board via a USB isolator (Linear technology) but failed. While, I can connect to the nucleo board directly without isolator and programme it. Beside, the PC can recognize the STLink from nucleo boa...

Resolved! STM32H745 EMC Behaviour internal Power

 Hello,I look for information, what is the best layout for the SMPS, which is included in the STM32H745. One of my problems is, for a proper design, you must consider to have small loops in the switching path.For my base layout, I used the same struc...

JPiet.3 by Associate III
  • 2213 Views
  • 2 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.