2024-12-01 10:22 PM
Hello,
Can I output an adjustable voltage ranging from -10V to 10V using the h753zi development board?
I found something like a "PWM to 0-5V/10V DAC Module."
Would I need to use such an external module or build an additional circuit externally to achieve this?
I would appreciate your advice and look forward to your response.
Thank you!
Solved! Go to Solution.
2024-12-01 11:38 PM
As the entire NUCLEO board operates with a positive voltage, a negative output voltage can only be achieved with external circuitry, which in turn also requires a negative supply voltage.
So yes, for ±10V you would have to connect a level shifter, e.g. using opamps.
Hope that helps?
Regards
/Peter
2024-12-01 11:38 PM
As the entire NUCLEO board operates with a positive voltage, a negative output voltage can only be achieved with external circuitry, which in turn also requires a negative supply voltage.
So yes, for ±10V you would have to connect a level shifter, e.g. using opamps.
Hope that helps?
Regards
/Peter
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.