2020-08-04 6:11 AM
Hello ,
According to the st25r95 datasheet:
"After the power supply is established at power-on, the ST25R95 waits for a low pulse on the pin IRQ_IN (t1) before automatically selecting the external interface (SPI) and entering Ready state after a delay".
I have a custom board and I want to read the device id over spi, but the IRQ_IN pin is not connected.
Can it work without IRQ_IN low pulse? Can I communicate with the device, currently I have nothing on MISO line.
Solved! Go to Solution.
2020-08-04 9:48 AM
Hi,
IRQ_IN needs to be connected and needs to follow the power up sequence. SPI communications can only be performed once the power up sequence is completed.
IRQ_OUT is recommended to be connected as well.
X-CUBE-NFC3 firmware uses both IRQ_IN and IRQ_OUT.
Rgds
BT
2020-08-04 9:48 AM
Hi,
IRQ_IN needs to be connected and needs to follow the power up sequence. SPI communications can only be performed once the power up sequence is completed.
IRQ_OUT is recommended to be connected as well.
X-CUBE-NFC3 firmware uses both IRQ_IN and IRQ_OUT.
Rgds
BT
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.