2024-08-21 8:47 PM - last edited on 2024-08-26 2:57 AM by mƎALLEm
Hello,
I'm using it with a custom board. I'm facing problem with switches the ST25R95 into low power consumption mode
When I send Calibrate command, it can work and return 0x78.
But if I send another command like wake up in IRQ_IN(07 0E 08 01 00 38 00 18 00 00 60 00 00 00 00 00) or tag detection(>0x07 0E 0A 21 00 79 01 18 00 20 60 60 70 80 3F 08),ST25R95 return me just 0xFD,I don't know why.
Kindly help me out.
Solved! Go to Solution.
2024-08-26 4:21 AM
HI,
can you confirm that your application relies on IRQ_OUT before reading the answer to the Idle command (see ST25R95 datasheet §5.9 "In low power consumption mode the device does not support SPI poll mechanism. Application has to rely on IRQ_OUT before reading the answer to the Idle command.")?
Also, I would recommend to base you application on top of the RF Abstraction Layer library provided in the ST25 embedded NFC library. It provides demos application and supports the tag detection.
Rgds
BT
2024-08-21 10:04 PM - edited 2024-08-26 1:21 AM
When I set it to wake up when timeout(0x07 0E 01 21 00 38 00 18 00 60 60 00 00 00 00 08) ,it return me {0x00,0x01,0x01},it is correct.
And I observed that after I sent (0x07 0E 0A A1 00 F8 01 18 00 00 60 60 00 00 3F 01 ) to calibrated the DacDataRef,
ST25R95 entered idle mode beacuse there was not any reaction when I placed the tag on top of the antenna.
Could you tell me why? thank you!
2024-08-26 1:22 AM
any warm heart person help me?
2024-08-26 3:00 AM
Hello @Eyzeryong ,
@Eyzeryong wrote:
any warm heart person help me?
You didn't receive an answer maybe because you didn't ask your question in the correct forum.
I moved your thread in ST25 NFC/RFID tags and readers.
2024-08-26 4:21 AM
HI,
can you confirm that your application relies on IRQ_OUT before reading the answer to the Idle command (see ST25R95 datasheet §5.9 "In low power consumption mode the device does not support SPI poll mechanism. Application has to rely on IRQ_OUT before reading the answer to the Idle command.")?
Also, I would recommend to base you application on top of the RF Abstraction Layer library provided in the ST25 embedded NFC library. It provides demos application and supports the tag detection.
Rgds
BT
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.