2020-07-01 4:24 AM
I have C1, 5 and 6 tags and I just need to enable energy harvesting so I can detect when tag is being read. Is there a simple way to do this, e.g. using the ST25 phone app. I have tried changing dyn register #1 but that did not work.
Please advise.
David
Solved! Go to Solution.
2020-07-01 8:53 AM
Hi @DAins.1 ,
This can be done with the ST25 NFC Tap Android application, but you need to change the static register instead to keep the Energy Harvesting enable after power on. The dynamic register (for EH) is used only to change dynamically the status of energy harvesting.
So you need to set the register EH_mode to 0 to keep energy harvesting always available.
Hope this can help you.
2020-07-01 8:53 AM
Hi @DAins.1 ,
This can be done with the ST25 NFC Tap Android application, but you need to change the static register instead to keep the Energy Harvesting enable after power on. The dynamic register (for EH) is used only to change dynamically the status of energy harvesting.
So you need to set the register EH_mode to 0 to keep energy harvesting always available.
Hope this can help you.
2020-07-02 3:11 AM
Hi Rene,
Perfect. I changed the register and got configuration password which I left at 00 and saved. All working.
David
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.