2021-09-28 2:52 AM
Hi,
How to calculate the ISO14443-a CRC value(16 bit). Please help me how to get the CRC.
ISO14443-A >>> CR95HFDLL_SENDRECEIVE, 300028
<< 8015 6A1E4DB17E00004B3592000000000000 9BC3 080000
0x9BC3 ISO14443-a CRC value
Kind Regards,
Merin
Solved! Go to Solution.
2021-09-28 4:36 AM
A Google search threw these...
A CRC function and links to others: https://stackoverflow.com/questions/40869293/iso-iec-14443a-crc-calcuation
Some details on CR95HF and clues where to get more: https://community.st.com/s/question/0D50X00009XkW7G/iso-14443a-cr95hf-and-the-crc-bit
Another CRC implementation: https://www.microchip.com/forums/m896426.aspx
Datasheets, tools and software: https://www.st.com/en/nfc/st25-nfc-rfid-tags-readers.html
2021-09-28 4:36 AM
A Google search threw these...
A CRC function and links to others: https://stackoverflow.com/questions/40869293/iso-iec-14443a-crc-calcuation
Some details on CR95HF and clues where to get more: https://community.st.com/s/question/0D50X00009XkW7G/iso-14443a-cr95hf-and-the-crc-bit
Another CRC implementation: https://www.microchip.com/forums/m896426.aspx
Datasheets, tools and software: https://www.st.com/en/nfc/st25-nfc-rfid-tags-readers.html
2021-09-28 5:50 AM
The resolved program to calculate the ISO14443-a CRC value(16 bit) as follow.
data_byte = 0x12;
CHECKSUM_CALCULATE(0x12 ^ 0x6363);
unsigned int CHECKSUM_DATA;
void CHECKSUM_CALCULATE(unsigned int C_DATA)
{
unsigned int n;
for(n=1;n<=8;n++)
{
if((C_DATA & 0x01)==0x01)
{
C_DATA = C_DATA >> 1;
C_DATA = C_DATA ^ 0x8408;
}
else
{
C_DATA = C_DATA >> 1;
}
}
CHECKSUM_DATA = C_DATA;
}
ISO14443A Polynomial is 0x8408, initial value is 0x6363, CRC output is 0x626d
online 16bit crc calculator : https://hub.zhovner.com/tools/nfc/
Kind Regards,
Merin
2021-09-28 6:29 AM
Hi,
just for my curiosity, why do you need to compute the CRC? The CR95HF does the job for you and provides a CRC error bit in the response flags of the SendReceive command.
Rgds
BT
2021-09-28 6:53 AM
The CRC here is 0xC39B in small endian form. If you run the data+crc thru the right shifting algorithm the data will divide cleanly resulting in a zero remainder.
C:\MSVC\CRC>iso14443a
626D == 0x626D
626D
test_one=C39B << Note High/Low bytes swapped
test_two=0000
PASS
// ISO14443A CRC Example sourcer32@gmail.com
#include <windows.h>
#include <stdio.h>
#include <stdlib.h>
typedef unsigned char uint8_t;
typedef unsigned short uint16_t;
typedef unsigned long uint32_t;
uint16_t crc_iso14443a(uint16_t crc, uint8_t data)
{
int i;
crc = crc ^ data;
for(i=0; i<8; i++)
if (crc & 1)
crc = (crc >> 1) ^ 0x8408;
else
crc >>= 1;
return(crc);
}
uint16_t crc_iso14443a_quick(uint16_t crc, uint8_t data)
{
static const uint16_t crctbl[] = { // 0x8408 Nibble Table, sourcer32@gmail.com
0x0000,0x1081,0x2102,0x3183,0x4204,0x5285,0x6306,0x7387,
0x8408,0x9489,0xA50A,0xB58B,0xC60C,0xD68D,0xE70E,0xF78F };
crc = crc ^ data;
crc = (crc >> 4) ^ crctbl[crc & 0xF]; // Two rounds of 4-bits
crc = (crc >> 4) ^ crctbl[crc & 0xF];
return(crc);
}
uint16_t crc_iso14443a_quick_block(uint16_t crc, int size, uint8_t *buffer)
{
while(size--)
crc = crc_iso14443a_quick(crc, *buffer++);
return(crc);
}
void test_one(void)
{
// ISO14443-A >>> CR95HFDLL_SENDRECEIVE, 300028
// << 8015 6A1E4DB17E00004B3592000000000000 9BC3 080000
uint8_t data[] = {
0x6A,0x1E,0x4D,0xB1,0x7E,0x00,0x00,0x4B,
0x35,0x92,0x00,0x00,0x00,0x00,0x00,0x00 };
uint16_t crc;
crc = crc_iso14443a_quick_block(0x6363, sizeof(data), data);
printf("test_one=%04X\n", crc );
}
void test_two(void)
{
// ISO14443-A >>> CR95HFDLL_SENDRECEIVE, 300028
// << 8015 6A1E4DB17E00004B3592000000000000 9BC3 080000
uint8_t data[] = {
0x6A,0x1E,0x4D,0xB1,0x7E,0x00,0x00,0x4B,
0x35,0x92,0x00,0x00,0x00,0x00,0x00,0x00,
0x9B,0xC3 };
uint16_t crc;
crc = crc_iso14443a_quick_block(0x6363, sizeof(data), data);
printf("test_two=%04X\n", crc);
if (crc == 0) puts("PASS"); else puts("!!FAIL!!");
}
int main(int argc, char **argv)
{
printf("%04X == 0x626D\n", crc_iso14443a(0x6363, 0x12) );
printf("%04X\n", crc_iso14443a_quick(0x6363, 0x12) );
test_one();
test_two();
return(1);
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.