2024-04-16 11:16 PM
Hello together
I am working on NDEF and mailbox communication between an Android smartphone and an X-Nucleo-NFC04A1 Eval Board. The Eval Board X-Nucleo-NFC04A1 communicates with a MB1717 STM32C031 board.
The embedded part works perfectly, the implementation was quick and easy thanks to the good lib you provide on the embedded page.
On the Android smartphone part (Android 14 with Google Pixel 6a) I have implemented your SDK with version ST25SKD-1.10.3 in a small test project. I have the project running with AndroidStudio and Gradle 8.7 without any errors.
But. It cannot recognise a single NFC tag. Whatever I try, it is unsuccessful. The function inten.getAction always returns a null. In the attachment I send you the small example project.
I have noticed that some deprecated functions are used in your Java class "TagDiscovery.java". Is there a newer version?
Could you please check where the error or my misunderstanding lies in the application?
Thank you very much.
RoM
Solved! Go to Solution.
2024-04-24 3:13 AM
Hello
Just change line 119 of main activity the
PendingIntent.FLAG_IMMUTABLEto
PendingIntent.FLAG_MUTABLEand you will discover Tags.
Concerning the class TagDiscovery.java, it is updates according to our released Tags.
Hope this help?
BR, FB
2024-04-24 3:13 AM
Hello
Just change line 119 of main activity the
PendingIntent.FLAG_IMMUTABLEto
PendingIntent.FLAG_MUTABLEand you will discover Tags.
Concerning the class TagDiscovery.java, it is updates according to our released Tags.
Hope this help?
BR, FB
2024-04-24 9:09 PM
Hi France
Thank you for your answer, I will check it out.
Kind regards
RoM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.