2018-06-27 12:22 AM
Hello,
I'd like to know what happen when to 2 tags of type 5 are in the vicinity of a reader ( par example a reader based on the X-NUCLEO-NFC05A1). The 2 tags can be detected simultaneously? Only the nearest tag will be detected? None of the tags will be detected because they will disturb each other?
#multiple-devices-simultaneously #nfc05 #tags-and-readers #nfc #tag-type-5Solved! Go to Solution.
2018-06-27 4:50 AM
Dear Fabrice,
Most NFC standards have a method implemented which is called anti-collision.
In fact, physically two tags / VICCs are interfering with each other and the reader / VCD has to detect and solve this collision. The methodology to do so is described in the according standard.
Please have a look at ISO/IEC 15693-3:2009 - 'Anticollision and transmission protocol' (chapter 8. Anticollision) for further details.
This anticollision procedure is already part of our X-NUCLEO-NFC05A1 software, therfore our demo kit can detect multiple tags / VICCs in vicinity.
BR Travis
2018-06-27 4:50 AM
Dear Fabrice,
Most NFC standards have a method implemented which is called anti-collision.
In fact, physically two tags / VICCs are interfering with each other and the reader / VCD has to detect and solve this collision. The methodology to do so is described in the according standard.
Please have a look at ISO/IEC 15693-3:2009 - 'Anticollision and transmission protocol' (chapter 8. Anticollision) for further details.
This anticollision procedure is already part of our X-NUCLEO-NFC05A1 software, therfore our demo kit can detect multiple tags / VICCs in vicinity.
BR Travis
2018-06-28 3:29 AM
Dear Travis,
Thank you for your answer.
I will try it
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.