2025-01-02 11:19 PM
Hello,
in the Datasheet of the STPM32 the accuracy of the active power is 0,1% error over 500:1 dynamic range.
Is this the best case error or the maximum error of the enerqy measurement after calibration?
What does the dynamic range of 5000:1 mean?
Solved! Go to Solution.
2025-01-06 1:38 AM
Hello,
The STPM32 accuracy is < 0.1% error over 5000 : 1 (not 500:1).
It means that for a given voltage (230 VAC for instance), the error on the measured Energy after calibration will stay < 0.1% for a current from 10mA (for instance) to 50A (considering a linear response of the current sensor).
The calibration has to be performed at 1 operating point only (typically the nominal values to be measured, 230V/5A for instance).
See AN4470 for details.
Best regards,
Didier Herrouin
2025-01-03 12:00 PM
Hello @Stp1
This post has been escalated to the ST Online Support Team for additional assistance. We'll contact you directly.
Regards,
Roger
2025-01-06 1:38 AM
Hello,
The STPM32 accuracy is < 0.1% error over 5000 : 1 (not 500:1).
It means that for a given voltage (230 VAC for instance), the error on the measured Energy after calibration will stay < 0.1% for a current from 10mA (for instance) to 50A (considering a linear response of the current sensor).
The calibration has to be performed at 1 operating point only (typically the nominal values to be measured, 230V/5A for instance).
See AN4470 for details.
Best regards,
Didier Herrouin
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.